Scheduled Maintenance We will be conducting scheduled maintenance on 17th of May from 10:00 PM EST to 18th of May​​ 9:00 PM EST. During this time MyAerospace applications will be temporarily unavailable. We apologize for any inconvenience this may cause.
Scheduled Maintenance Attention : Several of our website applications will be unavailable from Friday 05/03 08:30 PM EST through Sunday 05/05 08:30 AM EST due to Scheduled Maintenance as we work to improve performance. Thank you for your patience.
×

Your browser is not supported.

For the best experience, please access this site using the latest version of the following browsers:

Close This Window

By closing this window you acknowledge that your experience on this website may be degraded.

Honeywell Tests First T55-714C Engine

Honeywell Tests First T55-714C Engine

Chalk up another major achievement for Honeywell’s celebrated T55 turboshaft engine. The first T55-714C engine has reached the critical first engine to test (FETT) milestone on its way to being installed on a flight-test aircraft in support of the U.S. Army’s Cooperative Research and Development Agreement (CRADA).

Rigorous testing on the first and future T55-714C engines is planned over a two-year period to validate the benefits and ease of integration of the new engine variant onto the Chinook platform. Initial tests are being conducted in a specially designed test cell on the Honeywell engine campus in Phoenix.   

The new Honeywell engine will provide the Army with best-ever heavy-lift capabilities. The next-generation Chinook will be able to carry heavier loads, especially in high and hot operating conditions, than any previous version of the legendary helicopter.

The T55-714C engine is the latest version of the T55 turboshaft engine that has powered every Chinook flight since the first one in 1961. We celebrated the 60th anniversary of the helicopter’s first flight in October.   

The new engine will give the Chinook the power it needs to lift heavier payloads of troops, equipment and supplies, along with improvements in range and fuel efficiency. With the new Honeywell engine, the helicopter will carry up to 14,200 pounds of payload at 4,000 feet and 95 degrees F, compared to about 11,000 for the current CH-47.

The T55-714C will generate 6,000 shaft horsepower, which is a three-fold increase over the original T55 engine and a 20% improvement over the current T55-714A. In addition, the T55-714C will burn 8% less fuel and offer a 25% improvement in overall reliability, including 40% longer compressor life, thanks to a redesigned compressor module. 

Boeing is currently delivering Chinook aircraft equipped with the T55-714A engine, which can be seamlessly upgraded to the “C” version of the engine when production engines are available.

Aerospace Technologies Marketing

We inspire innovation. We are passionate and fearless inside and outside of work. We join forces and celebrate our global team. Now you can learn a little bit more about the amazing people that make up our culture at Honeywell Aerospace Technologies.

Comments

Please enter your name.
Please enter a valid email address
Please enter valid comment.